Failed to set modify trend properties - Time Period out of range
Failed to set modify trend properties. The
Time Period
is invalid. Enter a valid Time Period
in the range from 0 to 1000 * the specified Sample Period
.The maximum range for
Time Period
is limited to 1000 samples worth of data. Determine Max Time Period
by multiplying the Sample Period
(on the Sampling
tab) times 1000 Samples.Example: 10ms/Sample * 1000Sample * 1Sec/1000ms = 10 Seconds
The minimum range is zero.
Provide Feedback