Failed to paste from the system clipboard

Components are protected by License Source Protection
Could not paste the item into the project because one or more components are protected by License Source Protection, which is not supported on the selected controller in this version of the
Logix Designer
application.
To resolve the problem, try one of these options:
  • Remove License Source Protection from the components before pasting them.
  • Paste the component into a project on a
    ControlLogix
    5570 or
    CompactLogix
    5370 controller.
Remote modules configured as Listen Only cannot be pasted into this controller project
Cannot import remote modules configured as
Listen Only
from L5K/L5X files or pasted into a project on
CompactLogix
5380,
ControlLogix
5580,
Compact GuardLogix
5380, and
GuardLogix
5580 controllers
.
To resolve the problem, change the connection type in the
Module Definition
dialog and import the module again.
PlantPAx instructions are not supported by this controller type
Could not paste the item into the project because the item contains a PlantPAx instruction, which is not supported on the selected controller in this version of the
Logix Designer
Logix Designer
application.
TIP: For additional information on possible causes of a pasting error, check the
Errors
tab. To open or close the
Errors
tab, select
View > Errors
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal