Failed to set modify trend properties - Samples out of range
    Failed to set modify trend properties. The 
Samples 
value is invalid. Enter a valid Samples 
value that is a range from a low of 0 samples to a high of 1000 samples.Provide Feedback