Failed- obtain exclusive file access
    Failed to obtain exclusive file access required to conduct source control operation
This error appears when a writable version of the project file has been opened in another instance of the 
Logix Designer
 application. Close the initial version of the project file in order to open the project in the current instance of the application.Provide Feedback