Upload is not permitted from controller <controller name>.

Access has been denied. Check with your Security Administrator to be sure that you have access to the system.
Access Denied - Security Authority with ID < id > is required.
To Download to a controller that contains a project already bound to a Security Authority, you must be logged onto the FactoryTalk Directory to which the online project is bound. Refer to the Security tab help in the Controller Properties dialog for instructions on configuring a Security Authority.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal