Failed to open file <file name>

The specified project file could not be opened. The error message indicates one of the following conditions:
The FactoryTalk Directory does not contain the Logical Name: <Logical Name>
The project file is protected by a specific Logical Name that does not exist in the
FactoryTalk
Network Directory. Contact the security administrator to correct the problem.
The FactoryTalk Directory does not contain the Permission Set: <Permission Set>
The project file is protected by a specific permission set that does not exist in the
FactoryTalk
Network Directory. Contact the security administrator to correct the problem.
Access denied
Check with Security Administrator to verify access to the file.
The project file (ACD, L5K, L5X) is bound to a specific Security Authority or is protected by a specific permission set or Logical Name. To open the file, log onto the
FactoryTalk
Network Directory to which the project file is bound, or contact the security administrator to obtain access.
File not found
The file does not exist. If you selected a file from your most recent list under the
File
menu, it was deleted or moved since the last time you had it open. It will remain in the most recent list until it is replaced by other files as you open them.
Path doesn’t exist
You entered an incorrect path or the file does not exist in the specified path. Re-enter the correct path.
Not a project file
The file is not a
Logix Designer
application project file. Select a file with the .ACD extension. If you have files using this extension in your project directory that are not
Logix Designer
application projects, they should be moved or deleted to avoid confusion.
Invalid file extension
Project file names must use the .ACD extension; import/export files of entire projects must use the .L5K or .L5X extension. The
Logix Designer
application prevents creating project files with extensions other than .ACD, .L5K, .L5X, .AML, or .RDF. The application cannot open files that do not have one of these file extensions.
Project file too old
The file was created with an older, unsupported version of the
Logix Designer
application. This file cannot be converted. If you have the version of the application that it was created with, export it to an ASCII file and import it into the new version.
Project is already in use
The project file you specified is already open, either by you or by another user who is running the
Logix Designer
application.
Name is badly formed
The name does not follow the IEC-61131 naming standard. Enter an IEC-61131 compliant name.
Name too long
Logix Designer
application file names must be 40 characters or less in length. Rename the file with a shorter name to open the project.
Project file created with an engineering version of the
Logix Designer
application. Not intended for customer use.
The version of the application that created this project file was intended to be used only in the process of developing the
Logix Designer
application, and the project file cannot be converted to match a product version of the software.
Project file was created with a newer version of the
Logix Designer
application.
The version identifier in the project file is later than the version identifier used by this version of the software. The project file can only be opened by the version of the software that created it, or a later version. If you must, for some reason, try to open the project in this (older) version of the software, you must open it with the newer version, export it, and then try to edit the exported file.
Project file contains object that can't be converted
The project file contains an object in a format that can't be converted to work with this version of the
Logix Designer
application. To open this project, you must use the version of the application that created it, or the most current version of the application.
Timeout period expired
You do not have
RSLogix
5000 software v17 activated when you launch the software and try to open an
RSLogix
5000 software v16 ACD file. The grace period allows you to launch
RSLogix
5000 software v17, but not having that software activated prevents
RSLogix
5000 software v16 from launching and therefore causes
RSLogix
5000 software v17 to timeout.
You are trying to import a secured project file from an instance of the
Logix Designer
application that does not have security enabled.
The application must have security enabled and properly configured in order to be able to open secured project files. See your security administrator to have your workstation properly configured, or request a version of the project file that is not secured.
Cannot overwrite existing project file because its security information is either missing or inaccessible
The project does not have security information or the project is corrupt.
Required license is not available
The file could not be opened because one or more project components are protected, and the required licenses or source keys are not available. To resolve the problem, obtain the required licenses or source keys for the protected components.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal