Delete an alarm from the Alarm List

The
Alarm List
shows all the tag-based alarms in the project. Follow these steps to delete an alarm from the list.
To delete an alarm from the Alarm List:
  1. In the
    Controller Organizer
    , right-click
    Alarms
    and select
    Edit Alarms
    .
  2. Right-click an alarm in the list and select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal