Update controller parameters with the related tag values

Use the
Tags Import
tab of the
Import Export Manager
to update parameters in the ACM database with the related tag values in the Tag Configurator workbook. Typically, these values in the workbook are first uploaded from an online Logix Controller using Open Platform Communications (OPC). A Tag Configurator workbook can be used to change, download, and upload a controller's AOI or UDT instance tag values.
To update controller parameters with the related tag values
  1. Click
    TOOLS > Import Export Manager > Tags Import
    .
  2. In the
    Controller
    box, select a controller.
  3. In the
    Excel File
    box, either:
    • Enter the full path of the Tag Configurator workbook (.xlsm).
    • Click the ellipsis (...) button to browse to the file location.
  4. In the
    Configuration File
    box, either:
    • Enter the full path of the configuration file name (.xml).
    • Click the ellipsis (...) button to browse to the file location.
  5. Click
    Import
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal