Import a schedule
Use the
Import
tab of the Import Export Manager
to import objects (instances) and parameter values from a schedule (xlsx). Verify that the correct database name displays in the ACM title bar before starting the import process.
TIP:
When importing objects (instances), a compatible library (class) must be registered in the ACM database.
The Catalog Number of the registered library must match the Catalog Number in the schedule and a Library with a revision greater than or equal to the revision in the schedule must be registered.
If a library with the same revision is registered, the library with the same revision is used.
If a library with the same revision is not registered and a library with a greater revision is registered, the newest library is used.
If you see an Excel sensitivity label error message while importing a schedule, open
Excel and configure the sensitivity label. If the error message persists, contact your
organization's IT department for assistance.
To import a schedule
- ClickTOOLS > Import Export Manager. The most recently used project opens by default.
- To choose a different project to import, clickFILE > Openand then select the project from the list. If the ACM database does not contain any projects, theProjectbox is blank.
- Select the import method:
- New - Create a new projectUse to bring projects into a new ACM database.
- Replace - Overwrite projectUse to revert projects to a previously exported version.
- Update - Merge with existing projectUse to add content from other projects, or earlier versions of the same project, to the current project.
- Type a schedule file name (xlsx) in theExcel Filetext box or click the ellipsis to browse to the file.
- ClickImport.
- If you chooseReplace - Overwrite projectas the import method, theImportdialog opens.
- If you chooseNew - Create a new projectorUpdate - Merge with existing projectas the import method, theImport Completedialog opens.Errors, warnings, info, and debug log entries display.TIP:Filter the list of exceptions by clickingErrors,Warnings,Info, and/orDebug.
- (optional) ClickShow Log Fileon theImport Completedialog to display the entire contents of the most recent ACM log file in a text editor.
- If you choseReplace - Overwrite projectas the import method, clickNextto continue with the import and change the data in the Application Code Manager database.If you choseNew - Create a new projectorUpdate - Merge with existing projectas the import method, clickFinishto close theImport Completedialog.
- ClickFinishto close theImport Export Manager.
Provide Feedback