IAB / Architect tab settings
The
IAB / Architect
tab of the Import Export Manager
is used to create an ACM
partial import file containing Logix hardware modules that are configured in the Integrated
Architecture Builder (IAB) or Studio 5000 Architect.
IMPORTANT:
Select the EPlan XML export option when exporting the configuration file from IAB.
This table describes the settings on the
IAB / Architect
tab.Setting | Description |
|---|---|
IAB/Architect XML | Enter the full path of the configuration file (.xml) or click the ellipsis (...) button to browse to the file location. |
Convert | Create an ACM partial import file. |
Provide Feedback