Export tab settings

The
Export
tab of the
Import Export Manager
is used to export objects and parameter values to a schedule file.
This table describes the settings on the
Export
tab.
Setting
Description
All Projects
Select this option to export a schedule for each project in the connected ACM database.
A template cannot be applied.
Complete Project
Select this option to export a schedule for the current project.
A template can be applied to the export.
Partial
Select this option to export a schedule that includes only selected information from the current project.
With this option, these types of items can be specifically exported:
  • Controller
  • Hardware
  • Object
  • Library
Use Template
Select this checkbox to limit the items exported to the schedule using a schedule template.
When selected, choose to use either a
Local
,
Project
, or
Global
schedule template.
Show Modified
Select this checkbox to apply color codes in the schedule to denote "changed" (not equal to default) and "unchanged" (equal to default) parameter values.
Export Used Libraries
Includes all the associated library files for the project/controller in the export.
Export
Exports the schedule.
The
Export
button is available when a valid export configuration has been selected.
Export and Open
Exports the schedule and opens the schedule in Excel when the export is complete.
The
Export and Open
button is available when a valid
Complete Project
or
Partial
export configuration has been selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal