Create an ACM partial import file
Use the
IAB / Architect
tab of the Import Export Manager
to create an ACM
partial import file containing Logix hardware modules that are configured in the Integrated
Architecture Builder (IAB) or Studio 5000 Architect. The utility converts the IAB/Architect
(.xml) file to an ACM partial import file (.xlsx). Import the partial import file when a
corresponding ACM library exists in the database.To create an ACM partial import file
- ClickTOOLS > Import Export Manager > IAB / Architect.
- In theIAB / Architect XMLbox, either:
- Enter the full path of the configuration file (.xml).
- Click the ellipsis (...) button to browse to the file location.
- ClickConvert.
- InObject Configuration Wizard, configure properties of the imported file.
- ClickFinish.
Provide Feedback