Compare Tab settings
Use the
Compare
tab of the Import Export Manager
to compare the current project to a previously saved schedule.This table describes the settings on the
Compare
tab.Control | Description |
|---|---|
Only Show Changes | Select this checkbox to create a report that only lists the project content that has changed. |
Excel File | Click the ellipsis to identify the schedule file (*.xlsx) to compare with the current project. |
Compare | Compares the current project to the selected schedule file. The Compare button is available when a valid schedule has been selected. |
Cancel | Cancels the comparison. The Cancel button is available once the comparison is in progress. |
Previous | Not used. |
Next | Not used. |
Finish | Closes the tab. The Finish button is available once the comparison file has been created. |
Provide Feedback