Compare a project to a schedule
Use the
Compare
tab of the Import Export Manager
to compare the current project to a previously saved schedule file and create a report that highlights the differences.To compare a project to a saved schedule
- ClickTOOLS > Import Export Manager. The most recently used project is opened by default.
- To choose a different project to compare with, clickFILE > Openand then select the project from the list.
- Click theComparetab.
- InExcel File, type the name of the schedule file to use for comparison or click the ellipsis to browse to the schedule file.
- (optional) SelectOnly Show Changesto limit the content of the comparison report to items in the current project that differ from the schedule.
- ClickCompare.The comparison report opens in Excel.
- ClickFinishto close theImport Export Manager.
Provide Feedback