Log instruction

Logging may be added to templates with the following syntax:
##Log I am log message
It is important to note that all logging is removed from the template during generation. All log messages are written to the ACM log with level 'Debug'.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal