Comment instruction
Comments may be added to templates with the following syntax:
##! I am a comment
It is important to note that all comments are removed from the template during generation.
Provide Feedback
##! I am a comment