Delete an ACM database

Application Code Manager
(ACM) uses a database to store reusable code. At least one database is required.
To delete an ACM database
  1. Open
    Application Code Manager
    , in the main menu, click
    TOOLS > Database Manager
    .
  2. In
    Server name
    , select the computer name and
    SQL Server
    instance from the dropdown list or type a computer name and
    SQL Server
    instance in the following format:
    <Computer name>\<
    SQL Server
    instance>
  3. In
    Log on to the server
    , use Windows Authentication or type the
    User name
    and
    Password
    to use to authenticate the connection to the
    SQL Server
    , then click
    Connect
    .
    Status
    updates to
    Connected
    .
  4. In
    Specify the database
    , select the ACM database to delete.
  5. In
    Actions
    , select
    Delete database
    and then click
    Execute Task
    . The
    Confirm database delete
    dialog opens.
  6. Click
    Yes
    to confirm deletion of the database.
    Once the database is deleted, an
    Action completed successfully
    message displays. Click
    OK
    .
  7. Click
    Close
    to close
    Database Manager
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal