Database Manager settings
How do I open the Database Manager dialog?
- On the main menu, clickTOOLS > Database Manager.
The
Database Manager
dialog contains the settings that control how Application Code Manager
interacts with the SQL Server
database. It also
provides the ability to create, backup, and recover databases.This table describes the settings in the
Database Manager
dialog.Setting | Description |
|---|---|
Server name | Identifies the server that is hosting the SQL Server used by
ACM. Use the dropdown list to select a computer name and SQL Server instance from, or enter a computer name and SQL Server instance in the following format:<Computer name>\< SQL Server instance> |
Refresh | Queries the network for a list of SQL Server computer names
and instances and updates the selections available in the dropdown list with the
results. |
Log on to the server Using Windows Authentication or SQL Server Authentication(Note: This account and password are configured during installation of SQL Server .) | |
User name | The SQL Server user name associated with the ACM database.The default user name is "sa". |
Password | The SQL Server password associated with the user name.Starting with Application Code Manager version 5.01.00, the database password is
enhanced for security. For more information, see Enhanced SQL Server password management. |
ACM generated 'sa' password | Use the ACM generated 'sa' password instead of typing a password. |
Connect | When this button is clicked, Application Code Manager attempts to connect to
the database named in the Select a database name on the SQL Server entered in the Server name combo box. |
Status | Displays the result of the database connection attempt.
|
Specify the database | |
Select a database name | Identifies the database to manage. Enter a name or select an existing name from
the list. If the name entered is not present on the SQL Server ,
the option is provided to create a database. |
Tasks | |
Create database | Creates a database with the database name entered in the Select a database
name on the SQL Server entered in the Server name
when Execute Task is clicked. |
Upgrade database | Upgrades the ACM database named in the Select a database name combo box with the current schema when Execute Task is clicked. |
Delete database | Deletes the database named in Select a database name from the SQL Server identified in Server name when Execute
Task is clicked. |
Execute Task | Performs the selected task. |
Disaster Recovery | |
Backup database | Makes a backup copy of the database file named in Select a database name when Execute Recovery is clicked. |
Restore database | Replaces the database file named in Select a database name combo box with the backup database file when Execute Recovery is clicked. |
Execute Recovery | Performs the selected recovery. |
Provide Feedback