View registered library usage

There are several different reports that provide information about registered library usage. Determine the scope of the report by navigating to the level of interest and then generate the report.
To view registered library usage
  1. Select the scope of the report.
    • To generate a report that includes all of the registered libraries in the connected ACM database:
      Right-click
      Registered Libraries
      , then point to
      View
      , then click
      Library Usage
      .
    • To generate a report that includes all of the registered libraries used in a solution:
      In the
      Registered Libraries
      tree, right-click the solution folder, then point to
      View
      , then click
      Library Usage per Solution
      .
    • To generate a report that includes all of the registered libraries used in a library type:
      In the
      Registered Libraries
      tree, expand the solution folder, right-click the library type folder, then point to
      View
      , then click
      Library Usage per Library Type
      .
    • To generate a report that includes all of the registered libraries used in a library category:
      In the
      Registered Libraries
      tree, expand the solution folder, expand the library type folder, right-click the library category folder, then point to
      View
      , then click
      Library Usage per Library Category
      .
    • To generate a report that includes all of the registered libraries used for a library object:
      In the
      Registered Libraries
      tree, expand the solution folder, expand the library type folder, expand the library category folder, right-click the library object then point to
      View
      , then click
      Library Usage per Library
      .
  2. The selected report appears in a new window.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal