Register an ACM library object

Register an ACM library object to use it in a project.
Prerequisites
  • Verify that the ACM application is connected to the correct ACM database.
    TIP:
    The connected database is shown in parentheses in the
    Application Code Manager
    title bar.
To register an ACM library object
  1. In the
    Register Libraries
    tree, right-click the library object to register.
  2. Click
    Register
    .
  3. In the
    Open
    dialog, select your libraries, and then click
    Open
    .
  4. Review the information provided in the
    Library Registration
    window. Perform any indicated actions.
  5. Click
    Finish
    to complete the registration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal