Reconstitute an ACD file

Reconstitute an ACD file when the original
Logix Designer
project used to create the object is not available for editing. After reconstituting the ACD file, it can be edited using
Logix Designer
.
Hardware module libraries and ACM v1.x libraries do not support this feature.
To reconstitute an ACD file
  1. In the
    Registered Libraries
    tree view, right-click the library files.
    To select multiple files, hold down the
    Ctrl
    key and select the library files.
  2. Click
    Reconstitute ACD
    .
    The
    ACD Reconstitution Wizard
    opens.
  3. The
    Object Configuration
    page displays the details of the objects to be included in the ACD file.
    Click
    Next
    .
  4. The
    Resolve Dependencies
    page displays any dependencies between the library objects that must be resolved.
    • Click
      Add Dependency Library
      Add Dependency Library button and add the library that contains required Add-On Instructions (AOIs) or user-defined data types (UDTs).
    • Click
      Next
      .
  5. The
    Unresolved Names
    page displays any objects that have unresolved name values. Click in the
    Value
    column and type valid values for any names highlighted on the page then click
    Next
    .
  6. The
    L5X Generation Successful
    page displays a preview of the Logix content contained in the ACD file displays.
  7. Click
    Next
    to display the
    Save As
    dialog. In
    File name
    , type a file name for the ACD file.
  8. Click
    Save
    to save the file. The
    ACD successfully saved
    message displays with a link to open the folder where the file was saved.
  9. Click
    Finish
    to close the wizard.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal