Upgrade the application

When upgrading the
Application Code Manager
application, consider updating the libraries used in the ACM projects for a particular ACM database and obsoleting the previous version libraries.
IMPORTANT:
It is recommended to back up the current ACM database using the
Database Manager
before performing an upgrade. With the
Export Used Libraries
option enabled, export all projects using the Import Export Manager can also back up the database.
To upgrade the
Application Code Manager
application
  1. Install a newer version of
    Application Code Manager
    .
  2. Open
    Application Code Manager
    . A message appears with a prompt to upgrade the database. Click
    OK
    . The
    Database Manager
    displays.
  3. Select
    Upgrade database
    in the
    Actions - Tasks
    area and then click
    Execute Task
    .
    Click
    Close
    to close
    Database Manager
    .
  4. Right-click
    Registered Libraries
    and then select
    Register
    to ensure that any new libraries are added to the database.
    In the
    Open
    dialog, browse the default library file location.
    C:\Users\Public\Documents\Studio 5000\Libraries
  5. Open each folder. Select all the objects in the folder and then click
    Open
    .
  6. The
    Libraries Registration
    window opens and displays the status of the library registration process.
    Review any errors or warnings that were encountered.
    TIP:
    Results of the registration process are also saved to a log file. Click
    Show Log File
    to view the contents of the log file.
  7. Click
    Finish
    to close the
    Libraries Registration
    window.
    The registered libraries display in
    Application Code Manager
    under
    Registered Libraries
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal