Templates

A template defines the static content and format of the design output (for example, a
FactoryTalk View
display). A template is not a class definition. A template is not instantiated. Templates have a variety of formats (for example, xml, csv, docx, and xlsx) and are stored in the ACM program folder or an individual user folder.
Before a template can be used the initial configuration of ACM must be completed, the local library must be registered, and the template installed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal