Design Automation Concept

ACM generates the project design outputs automatically. The objects (instances) and parameter values, stored in the ACM database, are combined with various templates to create the following design outputs:
  • Logix
  • FactoryTalk View
    SE/ME graphics
  • FactoryTalk Historian
    SE import file
  • FactoryTalk Alarms and Events
    import file
  • Excel (Schedules)
  • FactoryTalk® Batch
    (Equipment editor)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal