Library Repositories
Library Repositories
displays the configured library repositories. A library repository refers to another ACM database that can be monitored for library updates. Libraries from these source databases can be easily replicated over to the currently active database for use within a project. It is unavailable to create an object directly from a library in a library repository. The library must first be replicated to the current active ACM database before it can be used to create an object. Add or remove library repositories in this pane.Click
View
and select Library Repositories
to open this pane.Right-click any branch in the
Library Repositories
tree view to view the commands available.This table describes each command. Commands appear at the applicable level of the tree.
Command | Description |
|---|---|
Library Repositories | |
Replicate to Active Database | Loads the Available Libraries form to select libraries to copy or register to the current active ACM database. |
Export | Exports the Library Repositories to an HSL4 (xml) formatted file. |
Extract Attached Files | Extracts the attached files to a folder. |
Disable All | Disables all update status checking of the databases. |
Add | Adds a library repository. |
Remove All | Removes all library repositories. |
Refresh | Refreshes all library repositories. |
Library repository nodes | |
Replicate to Active Database | Loads the Available Libraries form to select libraries to copy or register to the current ACM database. |
Export | Exports this library repository to an HSL4 (xml) formatted file. |
Extract Attached Files | Extracts the attached files of this library repository to a folder. |
Disable | Disables update status checking of this database. |
Remove | Removes this library repository. |
Connect | Sets this database as the current active database. |
Refresh | Refreshes all contents in this library repository. |
Solution, library type, and category branch | |
Replicate to Active Database | Loads the Available Libraries form to select libraries to copy or register to the current active ACM database. |
Export | Exports this branch to an HSL4 (xml) formatted file. |
Extract Attached Files | Extracts the attached files of this branch to a folder. |
Refresh | Refreshes all contents in this branch. |
Catalog number node | |
Replicate to Active Database | Loads the Available Libraries form to select libraries to copy or register to the current active ACM database. |
Export | Exports this library to an HSL4 (xml) formatted file. |
Extract Attached Files | Extracts the attached files in this library to a folder. |
Refresh | Refreshes this node. |
Provide Feedback