Generate command information

Use the help function in the ACM Console to provide detailed information about a specific command.
To generate detailed command information
  1. Type
    help
    then the full command and then press
    Enter
    .
    For example, type
    help exportproject
    , then press
    Enter
    .
    Detailed information on the
    exportproject
    command displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal