SubObject

The SubObject <ISObj> node represents a Sub Object. SubObject parameters must be supplied as <IPar> nodes within the child <IPars> node.
Parent node:
  • <ISObjs>
Child nodes:
  • <IPars>
    Attribute
    Description
    Name
    The name of the SubObject, such as
    Inp_Intlk01
    .
    Type
    The type of SubObject, such as
    Interlock
    .
    Description
    The description of the SubObject.
    OverrideDesc
    If formatting is applied to the SubObject description field in the library and this field is set to true, then the description can be overridden.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal