Parameter
The Parameter <IPar> node represents a library parameter.
Parent node:
- <IPars>AttributeDescriptionNameThe name of the parameter. This is a mandatory field and must be supplied.ValueThe value assigned to the parameter. This is a mandatory field and must be supplied.RefValThis attribute only applies to reference type parameters.If supplied, this value adds the reference to the parameter value, such as#refvalue.If not supplied, then a reference value is not added to the parameters value.
Provide Feedback