Interface Members

The Interface Member <IMem> node represents the configuration of an Interface Link member.
Parent node:
  • <IMems>
    Attribute
    Description
    Name
    The name of the Interface Member.
    Value
    The library instance name and output interface member to which to connect.
    RefVal
    The name of the output interface member in the destination library.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal