Interface Links
The Interface Links <IILink> node represents an interface link for a library instance. An Interface Link requires one <IMems> child node and one or more <IMem> grandchild nodes.
Parent node:
- <IObjs>
Child nodes:
- <IMems>AttributeDescriptionNameThe name of the interface link.KeyingCan either be specified asExactMatchorDisabled.ExactMatch: ACM matches input members against their respectiveKey IdandRevisionfield values.Disabled: ACM does not match input members against their respectiveKey IdandRevisionfield values.RefIntA reference to the library instance to which the Interface Link points.
Provide Feedback