Generate an example Extended script
Generate an example Extended script to copy and paste the XML structures and parameters to a new Extended script file for editing.
To generate an example Extended script
- Create a Project, Controller, and Object inApplication Code Manager.
- Generate an L5X controller file with theACM Project Dataoption enabled.
- Open the .L5X controller file in a text editor.
- Copy the <IObjs> and <ICOObjs> nodes to a new Extended script file.
Provide Feedback