When browsing a network, some connected devices do not appear

When I browse a network using the
RSLinx Classic
, why some of the devices that I know are connected to the network do not appear in the RSWho network topology?
When a device is configured in a CIP security zone with FactoryTalk Policy Manager,
RSLinx Classic
cannot communicate with that device. To communicate with the device, use a
FactoryTalk Linx
server that is configured in the same CIP security zone with the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal