What is a BOOTP server?

A BOOTP server or BOOTPS is software that detects BOOTP requests and transfers the needed configuration information for a device. Its configuration file contains a list of hardware addresses and their associated needs. Often this is just an IP address, but it can also have a file and directory associated with it. The PLC-5/E processors require only an IP address. The 5820-EI module requires an IP address and a binary file,
SGMPCCC.BIN
. In the case of the 5820-EI module, the BOOTP server must also have TFTP capability, to be able to transfer the file.
To open the BootP server:
  1. Click
    Windows Start
    .
  2. Select
    Rockwell Software
    >
    BootP-DHCP Tool
    >
    BootP-DHCP Tool
    TIP:
    The BootP-DHCP tool is configured together with RSLinx Classic.
Under UNIX, you would run a BOOTP daemon, which would always be running. Under DOS, you would probably run BOOTP server software when needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal