RSLinx Classic gives an error when reading a block of data from an SLC through a NetENI module

When using a NetENI module to communicate to an SLC be sure to uncheck the Use Maximum Packet Size (EtherNet) option displayed on the
Data Collection
tab of the DDE/OPC Topic Configuration window.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal