RSLinx Classic does not appear to be running

If RSLinx Classic is automatically started by COM (OPC clients) or by DTL32 (RSLogix products, custom C applications, and so on), no splash screen appears, and the RSLinx Classic main window is not shown. In this case, the RSLinx Classic application is said to be running "headless." RSLinx Classic does however appear as a system tray icon, just as if it were running as a service.
To view the existing RSLinx Classic, click the icon, right-click the icon and select Restore, or from the Start menu select
Programs > Rockwell Software > RSLinx > RSLinx Classic
. Any of these actions will bring the running RSLinx Classic to the foreground. To shut down RSLinx Classic, right-click the icon and select
Shutdown
, or right-click the icon, select
Restore
, and choose
File > Exit and Shutdown
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal