Can all INTERCHANGE Software applications be easily ported to RSLinx Classic?

In most cases, INTERCHANGE software applications can be ported to RSLinx Classic. Before creating the RSLinx Classic C API, Rockwell Software surveyed over 300 INTERCHANGE software users and all the major Independent Software Vendors that use INTERCHANGE software to find out what calls they were using. We found that most of them were using the same twenty or so calls. After implementing the 50 most popular calls, we found that about 98% of their applications could be supported.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal