All cells in a block requested contain the same data

Problem
When entering the required formula in Microsoft Excel (for example,
DDESHARENAME'T4:0.acc,L5,C1'
) to establish a hot link to read a block of data from a processor, the link is established, but the cells in the block requested contain the same data.
Solution
This formula is used to request five timer accumulators starting from
T4:0.ACC
. Microsoft Excel uses an array formula to represent the data, thus cells contain the value of the data for the first address (
T4:0.ACC
). To correctly display the data re-edit the range of cells and then use
Ctrl+Shift+Enter
to enter the data. This enters the data as an array formula. For more information on array formulas, please refer to the Microsoft Excel User's Guide.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal