Attempt to establish conversation failed; Start application RSLinx Classic error

Problem
When starting a client application, an error message shows: "Attempt to establish conversation failed; Start application RSLinx Classic".
Solution
There are two possible causes:
  • the topic name is misspelled
  • the topic does not point to a usable processor
Check whether the topic name is correct, and the topic points to a usable processor.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal