What should I do if my Visual Basic OPC application no longer compiles

With RSLinx Version 2.30.00 and later, the OPC Automation library was changed from RSLinxOPCAuto to RSIOPCAuto. If you have declared variables specifically to a given library such as RSLinxOPCAuto.OPCServer, a problem occurs. To correct this problem, change your data declarations to reference the new library (for example, RSIOPCAuto.OPCServer).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal