Name property

Description
(Read/Write) The name given to this group.
Syntax
Name
As String
Remarks
The name must be a unique group name, with respect to the naming of other groups created by this client.
If no name is specified, the server will generate a unique name for the group on the Add method of the OPCGroups object.
Example
'/* Change name of an existing OPCGroup
MyOPCGroup.Name = "ANewGroupName"
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal