Software compatibility
The DTL32.DLL Version 2.0 was built using Visual C++ compiler Version 5.0. It was tested with applications written using the following:
- Visual C++ Versions 4.1 and 5.0.
- Microsoft Visual Basic Versions 4.0 and 5.0.
- Borland C++ Versions 4.0 and 5.0.
Provide Feedback