Glossary
Activation file
- A hidden, read-only, system file that activates a Rockwell Software product. The software will run only if your system can find the correct activation file.Activation key -
Activation files contain a database of activation keys. Each key is particular to a certain product and must be accessible on a local or remote drive for that product to run.Driver -
The software interface to the hardware device that will be used to communicate between RSLinx Classic and your processor.DDE (Dynamic Data Exchange) -
A form of inter-process communication. When two or more programs that support DDE are running simultaneously, they can exchange information and commands.License
- Authorization to use a specified number of instances of software. A products activation key contains a license for each copy of the software you have purchased.Links -
The data path established for one or more channels between two or more stations. DDE links can be hot, warm, or cold.OPC -
Provides an industry-standard mechanism to communicate and exchange data between clients and servers using OLE technology.Packet -
The transmission unit exchanged at the network layer.Poke -
DDE version of a write.Read -
To acquire data from somewhere (memory, an output, another station).Topic -
Represents a specific path to a processor.Write -
To load data into somewhere (memory, an output, another station).Provide Feedback