Files installed

In addition to the RSLinx Classic OEM files, these development files were installed with the RSLinx Classic SDK in the
C:\Program Files\Rockwell Software\RSLinx\Samples
directory in one of the following subdirectories:
API\bcast.c
API\bcast.mak
API\cipconn.c
API\cipconn.mak
API\cipgetid.c
API\cipgetid.mak
API\cipmsg.c
API\cipmsg.mak
API\cipreg.c
API\cipreg.mak
API\dtl.bas
API\plc2.c
API\plc2.mak
API\readcb.c
API\readcb.mak
API\sample.c
API\sample.h
API\vlink.c
API\vlink.mak
OPC Automation\OPCBrowse.frm
OPC Automation\OPCBrowse.frx
OPC Automation\OPCBrowse.ico
OPC Automation\OPCQuality.bas
OPC Automation\RSLinxOPC.ico
OPC Automation\RSLinxOPCSample.frm
OPC Automation\RSLinxOPCSample.frx
OPC Automation\RSLinxOPCSample.vbp
OPC Automation\RSLinxOPCSample.vbw
OPC Custom\connect.mak
OPC Custom\ConnPt.cpp
OPC Custom\opc.h
OPC Custom\opc_i.c
OPC Custom\opccomn.h
OPC Custom\opccomn_i.c
OPC Custom\opcda.h
OPC Custom\opcda_i.c
OPC Custom\Readme.txt
OPC Custom\Sink.cpp
OPC Custom\Sink.h
OPC Custom\utils.cpp
OPC Custom\utils.h
OPCDOTNET\RSLinxNetSample.sln
OPCDOTNET\RSLinxNetSample.suo
OPCDOTNET\RSLinxNetSample\AssemblyInfo.vb
OPCDOTNET\RSLinxNetSample\OPCControl.vb
OPCDOTNET\RSLinxNetSample\RSLinxNetOPCSample.resx
OPCDOTNET\RSLinxNetSample\RSLinxNetOPCSample.vb
OPCDOTNET\RSLinxNetSample\RSLinxNetOPCSample.vbproj
OPCDOTNET\RSLinxNetSample\RSLinxNetOPCSample.vbproj.user
OPCDOTNET\RSLinxNetSample\Bin\RSLinxNetSample.exe
OPCDOTNET\RSLinxNetSample\Bin\RSLinxNetSample.pdb
TIP: If a directory named C:\ICOM or C:\RSI existed when you installed RSLinx Classic SDK, the development files will be installed in that directory instead of the
C:\Program Files\Rockwell Software
directory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal