Application notes
- You can now configure the conversion function DTL_GET_SLC500_FLT to not alter the input buffer. See DTL_SETOPT for details.
- The DTL32.LIB import library supplied with RSLinx Classic SDK and the Borland C++ compiler are not compatible. If you are using Borland C++ 5.0, you must create your own import library using the IMPLIB utility supplied with the compiler to be compatible with the Borland compiler. The syntax to run the utility isIMPLIB dtl32.lib %systemroot%\system32\dtl32.dllYou can also run IMPLIB without parameters to display all options for the utility.
- Not all MicroLogix 1500 data types are supported by the DTL_C_DEFINE function.
Provide Feedback