DTL_TODTSA parameters
name_id
is the handle that was returned when the data item was defined using DTL_C_DEFINE.address
is a pointer to a DTSA_DH, DTSA_DH_R, DTSA_BKPLN, DTSA_AB_DH_LOCAL, DTSA_AB_DH_OFFLINK, DTSA_AB_PIGATEWAY, or DTSA_AB_DF1MASTER structure that is used to uniquely define a communication path to a local chassis or a remote processor. Its type must be cast to DTSA_TYPE when calling this function.Provide Feedback