DTL_TODTSA comments
The DTL_TODTSA function creates a DTSA_TYPE structured address given the
name_id
of a solicited data item.If
name_id
was obtained from the definition of a remote solicited data item, a DTSA_TYP_DH, DTSA_TYP_DH_R, DTSA_AB_DH_OFFLINK, DTSA_AB_PIGATEWAY, or DTSA_AB_DF1MASTER structured address is returned in address.If
name_id
was obtained from the definition of a local solicited data item or an unsolicited data item, a DTSA_TYP_BKPLN or DTSA_TYP_AB_DH_LOCAL structured address is returned in address
. The module, pushwheel, and channel fields of the DTSA_TYP_BKPLN structured address are zero.Provide Feedback