DTL DISCONNECT comments

Once DTL_DISCONNECT has been called, RSLinx Classic software no longer calls the event handler associated with the specified network interface. Any pending solicited I/O operations for this
ni_id
are completed with an I/O completion status (
io_stat
) of DTL_E_DISCONNECT. After the disconnect function call completes, attempts by the client application to initiate an I/O operation using this
ni_id
fails. The return value is DTL_E_NOTCONNECT and the final I/O completion status is DTL_E_NOATMPT.
Any subsequent unsolicited I/O operations sent to this
ni_id
are rejected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal