DTL_GET_WORD
The DTL_GET_WORD function converts the specified value from processor data type SIGNED WORD (PLC-3, PLC-5, PLC-5/250, SLC 500, SLC 5/03, or SLC 5/04) to application data type WORD.
SHORT DTL_GET_WORD(
in
)UNSIGNED CHAR * in ; | /* pointer to input buffer |
Provide Feedback