DTL_CIP_CONNECTION_CLOSE parameters

conn_id
is the connection handle obtained from a previous DTL_CIP_CONNECTION_OPEN call made by the application, or from execution of a registered application's DTL_CIP_APPLICATION_CONNECT_PROC callback function (see DTL_CIP_APPLICATION_REGISTER).
timeout
is the maximum time (in milliseconds) to wait for the connection to close cleanly.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal