DTL_CIP_CONNECTION_REJECT parameters

conn_id
is the connection handle provided in the DTL_CIP_APPLICATION_CONNECT_PROC call.
return_status
is the CIP-defined status code to be returned. It should normally be 0x01.
ext_buf
is a pointer to a buffer containing the extended status to be returned. It should normally be a two-byte
reason code
.
ext_size
is the size in bytes of the contents of
ext_buf
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal